Search FAQs
What is the minimum Vijeo Designer version which will program the HMISTU series?
Issue:
Unable to download to my brand new HMISTU855 or HMISTU655 with Vijeo Designer
Product Line:
HMISTU Series, HMISTU655, HMISTU855, HMIS5T
Resolution:
For HMIS5T rear modules with PV:09 RL.16 SV:6.0 or greater, we must use Vijeo Designer 6.2 SP7 or greater. For any PV, RL, SV numbers that are older we can use Vijeo Designer 6.2 SP6 or older. The minimum version is Vijeo Designer 5.1 SP2.
Unable to download to my brand new HMISTU855 or HMISTU655 with Vijeo Designer
Product Line:
HMISTU Series, HMISTU655, HMISTU855, HMIS5T
Resolution:
For HMIS5T rear modules with PV:09 RL.16 SV:6.0 or greater, we must use Vijeo Designer 6.2 SP7 or greater. For any PV, RL, SV numbers that are older we can use Vijeo Designer 6.2 SP6 or older. The minimum version is Vijeo Designer 5.1 SP2.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: