Issue: Is it possible to use an output contactor to open the motor circuit on the ATV12?
Product Line: ATV12
Environment: All
Cause: ATV12 and Output contactor
Resolution:
The ATV12 has been designed to support this kind of application without any particular precaution (without ferrite...).
So you can add an output contactor directly between the motor and the drive and open it even if the motor is loaded