{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for a Magelis XBTF034510?

Article available in these languages: Spanish

The hardware replacement for a Magelis XBTF034510 is the Magelis HMIGTO5310 (TouchScreen) & XBTZGCO3 (Cut Out Adapter).
The software to program the Magelis HMIGTO5310 is Vijeo Designer and the part number with cable is VJDSUDTGAV62M.

Note: The adapter plate is only needed when replacing an existing XBTF terminal.


Schneider Electric Nigeria