{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I connect to the Quantum 140CPU11302 using EcoStruxure Control Expert?

Issue:
I am attempting to connect to the 140CPU11302 with Unity Pro and I keep getting an error.

Product Line:
Quantum PLC

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution:
You can not connect to the Quantum 140CPU11302 with Control Expert or Unity Pro. This is a 984 Quantum and you can only program it using ProWorx NxT, ProWorx 32, or Concept.

Schneider Electric Nigeria