No, the embedded IO ( DM72F0, DM72F1, DI12DE, DO12TE and AI4LE) are part of the controller and are not field replaceable. The whole controller must be replaced.
Released for:Schneider Electric Nigeria
Explore more
Range:
Modicon TM5
Modicon M258
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.