undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
When creating a located variable of data type REAL in an M340 or M580 application, is there an addressing restriction?

Yes. When programming an M340 or M580 application with Unity Pro, the located REAL variables must be assigned EVEN starting addresses such as %MW2 .%MW4, %MW50 . Addresses using
odd numbers such as %MW1, %MW3 or %MW49 would not be acceptable. Any 32 bit data type would have to follow this regimen. (DINT,DWORD,etc)


Legacy KB System (APS) Data: RESL212622 V1.0, Originally authored by DaSo on 09/27/2013, Last Edited by DaSo on 09/27/2013
Related ranges: Unity Pro - SoCollaborative software

Schneider Electric Nigeria

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: