Search FAQs
Can I change the IP address of the Magelis in Vijeo Designer and download the changes over ethernet?
Issue:
Changing the IP address of the Magelis in Vijeo Designer and download the changes over ethernet
Product Line:
Vijeo Designer
Resolution:
No, It's not possible to change the IP address of the Magelis from Vijeo Designer and still download over ethernet.
To make changes to the IP address, you have to download either via USB cable or file system.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: