{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Communication on Modbus TCP/IP of Premium and XBTG range.

Goals and Symptoms

Configuration of the application :
Premium + ETY using Modbus TCP/IP protocol to communicate with an XBTG product range.
The exchange of bits %Mi between XBTG and premium generate an error code 02H

Causes and Fixes

The workaround is the limit of the Prefered Frame Length to 120. This value could be defined by Vijeo Designer to a minimum or maximum Possible. But if you clic on the field array and write 120. This will limit the length of the frame exchanged between XBTG and Premium to the maximum value supported by premium.
We will keep we informed as soon as this issue is corrected


Legacy KB System (APS) Data: RESL176540 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT G

Schneider Electric Nigeria