Search FAQs
How to use the sin-ramp type in a LMC20 CNC-application?
Goals and Symptoms
How to use the sin-ramp type in a LMC20 CNC-application?
Causes and Fixes
The ramp-type settings in the drive-configuration works only for single axis movements (for example MC_MoveAbsolute,....). For CNC-application (Using of SMC_Interpolator and SMC_ControlAxisByPos, the input "iVelMode" of the Interpolator needs to set to "1". Different jerk values are not possible.
Legacy KB System (APS) Data: RESL202091 V1.0, Originally authored by JoAr on 04/23/2010, Last Edited by JoAr on 04/23/2010
Related ranges: Lexium Controller LMC10 - LMC20
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: