{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can we drain the gear oil in an ILE1B661TC1A8? What is the reference of the gear oil? --------------------------------------------------------------...

Goals and Symptoms

Can we drain the gear oil in an ILE1B661TC1A8?
What is the reference of the gear oil?
-------------------------------------------------------------------
Peux t'on vidanger l'huile du réducteur d'un ILE1B661TC1A8 ?
Quelle est la référence de l'huile du réducteur ?

Causes and Fixes

Klüberplex BEM 34 - 132 special grease ( see attachment )

Attachments

(Removed File URL: 202985_FB46/Kl_C3_BCberplex_BEM34-132.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/78593e61bc029fd0c12577730052a84a/fl_block_5/0.602?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL202985 V1.0, Originally authored by VoKo on 08/02/2010, Last Edited by VoKo on 08/02/2010
Related ranges: Lexium ILA, ILE, ILS

Schneider Electric Nigeria

Attachment(s)
Kl_C3_BCberplex_BEM34-132.pdf [165.7 KB]