{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to use Lexium32 limit switches for TwinCAT NC-homing (Lexium32-EtherCAT)

Goals and Symptoms

How to use Lexium32 limit switches for TwinCAT NC-homing (Lexium32-EtherCAT)

Causes and Fixes

Before the MC_Home will be started, it is required to disable the limit switches in the drive temporary by object 3006:11h. The state of the digital IO can be mapped into the PDO and linked into the PLC-program (for using it on input bCalibrationCAM on MC_Home)

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.