{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the mean time between failures (MTBF) for older ConneXium product?


This table reflects the mean time between failures in hours for each of the older ConneXium PRODUCTS. If you divide the total hours by 8760 (number of hours in a year), you will get the total number of years between failures. If you divide 720 (hours in a month) you will have the total months between failures.

ConneXium

Part NumberDescription
MTBF in Hours
499NEH00410DIN Rail 10Base-TP Hub (4 10Base-T RJ45 Ports)
1,399,091
499NEH04100DIN Rail 100Base-TX Hub (4 100Base-TX RJ45 Ports)
1,182,145
499NEH00510DIN Rail 10Base-TP/FL Hub (3 10BaseT RJ45, 2 10BaseFL ST Multimode Ports)
347,000
499NOS07100DIN Rail 10/100 Base-TX/FX Switch (5 10/100 RJ45, 2 Redundant Duplex SC Multimode Ports)
171,000
499NES07100DIN Rail 10/100 Base-TX/TX Switch (5 10/100 RJ45, 2 Redundant RJ45 Ports)
177,000
499NES08100DIN Rail 10/100Base-TX Switch (8 10/100Base-TX RJ45 Ports)
454,000
499NTR00010DIN Rail 10Base-TP/FL Transceiver, Multimode
1,196,387
499NTR00100DIN Rail 100Base-TX/FX Transceiver, Multimode
1,200,523

Legacy KB System (APS) Data: RESL120001 V2.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet

Schneider Electric Nigeria