{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
We have an softstarter ATS48C48Q that is displaying the OCF code. We have been following the instruction on User´s Manual : checking the motor and wir...

Goals and Symptoms

We have an softstarter ATS48C48Q that is displaying the OCF code. We have been following the instruction on User´s Manual : checking the motor and wire isolation, by-pass circuits testing, and the others instrucctions. We didn´t find anything that explains the situation. The OCF code is displayed randomly, in anytime, inclusive without the RUN command actived and without the power supply L1-L2-L3 conected. Could you say us what antohers causes are posible? We already have changed the control board, but the result is the same : the OCF code continues diplaying.

Facts and Changes

OCF

Causes and Fixes

Try to replace the power board because a bad solding is also possible, or the best way is to replace the complet product.


Legacy KB System (APS) Data: RESL156439 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48

Schneider Electric Nigeria