{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the derating factor used when sizing LH4N for a high number of starts per hour than the standard spec of 360 seconds.

Goals and Symptoms

What is the derating factor used when sizing LH4N for a high number of starts per hour than the standard spec of 360 seconds.

Facts and Changes

LH4N Starts/hour
starting

Causes and Fixes

There is not studies which gives a factor to determine the power of LH4 in an application with high number start/stop per hour upper her electrical characteristics of the product.
The catalogue tell you :
-'' if starting and stopping conditions are severe, or if the starting current must be controlled, it is preferable to use an ATS48 unit''.
- ''beyond this starting duty, the start unit must be derated by one size''.

However , we thinks when the number of start/stop is considerable and it would have been preferable to use a variable speed drive.

Note:  The LH4 softstart family is obsolete. It was replaced by the ATS01 softstart, or in the case of the larger LH4's the ATS22.


Legacy KB System (APS) Data: RESL160232 V1.0, Originally authored by on , Last Edited by on
Related ranges: LH7, LH4

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: