{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the Advantys STBXMP1100 bus termination plate have to be ordered separately?

Issue:
Does the Advantys bus termination plate STBXMP1100 come with the NIM module or does it have to be ordered separately?

Product Line:
Advantys

Environment:
Advantys Configuration Software

Cause:
Customer not sure if they lost the termination plate and if it comes with it or if it has to be ordered separately.

Resolution:
The Advantys bus termination plate does not have to be ordered separately. The bus termination plate is shipped with each NIM module, however, a replacement bus termination plate can be ordered as part number: STBXMP1100.

Schneider Electric Nigeria