undefined undefined
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
How can we help you today?
How do I Configure the Slot ID in a Quantum 140-CPU-6xx-xx Ethernet configuration?


The high byte of fifth configuration register for the MBP_MSTR block is used to define which backplane slot position the Ethernet module resides in
the older Quantum controllers had a single slot Ethernet head module so the high byte of that register would be set to the slot number in which the NOE resides.


The new Quantum 140-CPU-6xx-xx controllers have a built-in Ethernet port and the controller itself is two slots wide.

The high byte is not set to either slot three nor slot four; rather a code of FE Hex is used to indicate the block be directed out of the native Ethernet port on the CPU.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.