{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the pinout of the TSXCPU1030, TSXCPU1031 programing cable?

 

image0

8 Pin mini-din
1. D (B) RS 485
2. D (A) RS 485
3. Not Used
4. Negative Data Transmit Enable
5. TER port mode control
6. Not Used
7. GND 0V
8. Logical VCC

9 Pin SubD
1.DCD
2. Rx
3. Tx
4. DTR
5. Signal Ground
6. Not Used
7. RTS
8. CTS
9. Not Used

User-built cables are possible, but not recommended. An example below of a user-built cable employing a B&B Electronics RS232 - 485 converter (MN: 485LDRC) is shown below:
image1

The dip switches on the converter are set to as follows:
1 Up, 2 Up, 3 Up, 4 Up, 5 Down, 6 Up, 7 Down, 8 Down

Legacy KB System (APS) Data: RESL162737 V1.0, Originally authored by on , Last Edited by on
Related ranges: Uni-Telway

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.