{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
If a program is developed in the ProWorx 32 software, can it be converted back to ProWorx NxT?

Issue

If a program is developed in the ProWorx 32 software, can it be converted back to ProWorx NxT?

Product Line

ProWORX

Environment

ProWorx NxT

Resolution

Yes, you can convert a ProWorx 32 database back to ProWorx NxT. First, open your ProWorx 32 project. Select "FILE", then "EXPORT TO NXT". Choose a destination folder, create a File Name, then click on the SAVE button.

Schneider Electric Nigeria