Search FAQs
What is the difference between the Compact AS-BFRQ-204 and the AS-BFRQ-254 frequency modules?
Issue
What is the difference between the Compact AS-BFRQ-204 and the AS-BFRQ-254 frequency modules?
Product Line
Compact
Environment
AS-BFRQ-204
Resolution
The only difference between the two Compact frequency modules is that the AS-BFRQ-254 module operates at extended temperatures.
Operating Temperature:
AS-BFRQ-204.....0 to +60 degrees C
AS-BFRQ-254.....-40 to +70 degrees C
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: