{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Connection lost between the Unity-Pro PC and the PLC just after the Run command through the USB driver

Symptoms

The Unity-Pro project is transferred through the USB port and the connection is lost just after the Run command.
The animation remains frozen and the following message is displayed :
"PLC failed - Automatic return to off line"

The PLC remains in Run mode, every time you try to connect it again the same message is displayed.

How to fix

The connection is lost because the project has a long Scan Time and the request takes more time than the driver timeout to get an answer.

You have to change the timeout of the driver, for that :
- Under Unity-Pro, select in the menu PLC -> Set Address,

Setting PLC Address

- In the PLC area, click on the "Communication Parameters" button,

PLC Communication Timeout Parameter
You can increase the Timeout to 10 seconds in order to stay connected.

-Click OK to validate.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.