Search FAQs
What is the replacement for the Modbus Plus ISA adapter AM-SA85-000 (single channel)?
Issue
What is the replacement for the Modbus Plus ISA adapter AM-SA85-000 (single cable)?
Product Line
Modbus Plus
Environment
AM-SA85-000
Resolution
The Modbus Plus ISA-SA85 adapter (AM-SA85-000) has been replaced with the (AM-SA85-030). This is basically the same Modbus Plus single channel adapter card. Part number AM-SA85-000, which included just the adapter is no longer actively sold. We now sell part number AM-SA85-030 which is a kit that includes both the adapter (AM-SA85-000) along with the latest version of the Modbus Plus driver suite CD.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: