{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do I read or write a program to/from the SY/MAX model 50 controller's memory pack to the 8005PR4 hand held programmer's PROM burner socket?

Issue

How do I read or write a program to/from the SY/MAX model 50 controller's memory pack to the 8005PR4 hand held programmer's PROM burner socket?

Product Line

SY/MAX

Environment

8005PR4

Resolution

First ensure you have the memory pack installed in the 8005PR4's PROM burner socket.
To read a program from the SY/MAX model 50 controller's memory pack to the 8005PR4 enter the following sequence:

  1. PROM, READ.
  2. Once "PROM READ GO?" is displayed press the ENTR key. "PROM READ" is displayed during execution.
  3. When completed "PROM READ END" is displayed.


To write a program from the 8005PR4 to the SY/MAX model 50 controller's memory pack enter the following sequence:

  1. PROM ENTR.
  2. Once "PROM WRIT GO?" is displayed press the ENTR key. "PROM WRIT" is displayed during execution.
  3. When completed "PROM WRIT END" is displayed.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: