{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why don't I have the option for TCP/IP in the ProWorx NxT Configuration Extension for the Quantum 140CPU11302 and 140CPU11303 controllers?

Issue

Why don't I have the option for TCP/IP in the ProWorx NxT Configuration Extension for the Quantum 140CPU11302 and the 140CPU11303 controllers?

Product Line

Quantum, ProWorx NxT

Environment

ProWorx NxT, 140CPU11302

Resolution

The problem is the wrong REV controller has been selected. The TCP/IP option is only available for the Quantum 140CPU11302 and 140CPU11303 REV 2 controllers. The TCP/IP option is not available for the REV 1 controllers in the NxT Add Configuration Extension window.

Schneider Electric Nigeria