Search FAQs
How can the program be loaded from the EEPROM cartridge to a TSX17?
Issue
How can the program be loaded from the EEPROM cartidge to a TSX17?
Product Line
TSX7 Micro
Environment
TSX17
Resolution
The EEPROM cartridge has a micro switch on it. The micro switch needs to be in the Master (left most) position. With the switch in this position the controller will load from the EEPROM on power up.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: