Search FAQs
How do I get Modsoft to open up to full screen display while I try to run it under WIN 2000?
Issue
How do I get Modsoft to open up to full screen display while I try to run it under WIN 2000?
Product line
Modsoft
Environment
Modsoft, Windows 2000
Resolution
The command to get Modsoft to change window size is ALT+<ENTER>; however Modsoft is not supported under WIN 2000. Users may try running the application under it; however successful operation cannot be guaranteed. One of the common problems is Modsoft will not open up to full screen. Regrettably there is no means to resolve this issue other than to reinstall the software under a supported OS, such as WIN 95, WIN 98 or DOS.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: