{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do we determine the maximum point of encoder ?

Goals and Symptoms

How do we determine the maximum point of encoder ?

Facts and Changes

ATV71
Codeur
Encoder

Causes and Fixes

Fmax = 300 Khz
Maximum point of encoder = 5000

The formule is :
Encodeur point = 1/rpm x Fmax x 60, rpm is the speed of the motor.

Example : Motor 50Hz 2830 tr/mn using at 110Hz then 6226 tr/mn
The calcul done = 2891 it must take a 2048 point


Legacy KB System (APS) Data: RESL173103 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 71

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: