{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
171CCC9x030 M1E Processor IEC Firmware Upgrade to v.1.26

Issue
The purpose of this resolution is to inform Momentum M1E users that the IEC firmware has been upgraded to version 1.26.


Product Line
Momentum
171CCC98030
171CCC96030


Environment


Resolution
Firmware v.1.26 resolves an issue with pinging an M1E through a router across a WAN. This problem also occurred in IEC Exec. versions 1.21, 1.22, and 1.23.

Note: It is recommended to power cycle the M1E immediately after downloading the firmware and before loading a configuration.

Schneider Electric Nigeria

Attachment(s)
M1ev126e.zip [232.13 KB]