Search FAQs
STB Island Module Hot-Swapping Information
Issue
The purpose of this resolution is to inform STB users of a point regarding hot swapping the islands I/O modules.
Product Line
Advantys,STB
Resolution
STB design does not allow hot-swapping of an I/O module if there is only one module in the island. The same is true if you have multiple modules and you remove all of them prior to replacing one. The NIM will enter fatal error and require a power cycle to resume operation once the module is replaced.
Legacy KB System (APS) Data: RESL176389 V1.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: