{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Ethernet NIM Diagnostic Register Corrective Actions

Issue

The purpose of this resolution is to suggest corrective actions which may be taken in the event error indications are displayed in the Ethernet NIM Diagnostic registers.

Product Line
Advantys, STB

Resolution

Reference the attachment Diagnostic Data Corrective Actions for recommendations in the event errors are displayed in the STBNIP2212 Ethernet NIM Diagnostic registers. A description of the registers may be found in the Advantys STB Ethernet Modbus TCP\IP Network Interface Applications Guide, p/n 890USE17700, Data Exchange Chapter 6, Reading Diagnostic Data.

Schneider Electric Nigeria

Attachment(s)
Diagnostic_Data_Corrective_Actions.zip [2.8 KB]