{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
140NOE77110 Firmware Upgrade to v.3.5

Issue
This resolution was edited on May 23, 2006 to correct the part number from a 140NOE771x0 to a 140NOE77110 only.


Product Line
Quantum
140NOE77110


Resolution
The purpose of this resolution is to inform 140NOE77110 users that the firmware has been upgraded to version 3.5.

A user has the ethernet cable inadvertently disconnected from an NOE77110 while logged in. Attempting to log back in after re-connecting the cable would fail, with the error "User Already Logged In".  Firmware  v.3.5 now allows the user to re-connect without an error.

Schneider Electric Nigeria