{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I find the unknown IP address of a Modbus Serial-to-TCP Gateway?

Issue:
How to find the unknown IP address of a Modbus Serial-to-TCP Gateway?

Product Line:
EGX100
ETG100
EGX300
EGX150 (Link 150)
Com'X

Environment:
Internet Explorer
WireShark

Resolution:
The lost IP address of a Modbus Serial-to-TCP Gateway can be found by examining the
WireShark trace of the Ethernet TCP/IP communications using the following steps.
This method can also be used for mostly any ethernet-based device.

  • Download WireShark from https://www.wireshark.org/download.html
  • Launch WireShark
  • Select the active Ethernet adapter on the PC to start the WireShark trace.
  • Power-Cycle the Modbus Serial-to-TCP Gateway.
    When the Gateway reboots, it will send a Gratuitous ARP from the MAC Address with the IP address of the gateway which can be seen in the trace.
  • Confirm this is the IP address by using an Internet Explorer browser to connect to the embedded web pages on the gateway.

Schneider Electric Nigeria