Release Notice
Connection issue between PL7 PRO with XIP driver to TSX MICRO connected on Ethernet with TSX ETZ 510
Goals and Symptoms
After a communication closure with TSX PREMIUM, then opening a new one with a TSX MICRO, without the closure of PL7 PRO, it is impossible to connect to the TSX MICRO.
Causes and Fixes
Solution 1: Close PL7, open again, define address of TSX MICRO, connection: OK
Solution 2: Without closure of PL7, create new PLC TSX MICRO, define address of PLC, connection: OK
Legacy KB System (APS) Data: RESL179251 V1.0, Originally authored by on , Last Edited by on
Related ranges: PL7
Released for:Schneider Electric Nigeria