{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
RS485 Communication Wiring Diagram for a Momentum Processor to a Merlin Gerin Digipact DC150

Issue
The purpose of this resolution is to diagram the RS485 wiring for Modbus communications between a Momentum processor and a Merlin Gerin DC150. The RS485 pinout shown in the DC150 User Manual is incorrect.

All Momentum Processors can be used in this application. The following have a builtin Modbus RS485 communications port and do not require a 172JNN21032:
· 171CCC98020
· 171CCC98030
· 171CCS78000
· 171CCC78010


The following Momentum Processors do not have a builtin Modbus RS485 port and requires a 172JNN21032 Option Adapter to work in this application:
· 171CCS70000
· 171CCS70010
· 171CCS76000
· 171CCC76010
· 171CCC96020
· 171CCC96030


The Data Concentrator is:
· Merlin Gerin Digipact DC150

Product Line
Momentum
Merlin Gerin Digipact DC150


Environment


Resolution
RS485 wiring from a Momentum processor (port 2, db9) to a Merlin Gerin DC150.



NOTE: The signal pinouts for the db9 RS485 connector as shown in the Merlin Gerin DC150 User Manual are incorrect. The correct pinouts are shown above.
______________________________________________________________________________

  • RS485 wiring from a Momentum 172JNN21032 Option adapter (port 2, RJ45) to a Merlin Gerin DC150.

NOTE: The signal pinouts for the db9 RS485 connector as shown in the Merlin Gerin DC150 User Manual are incorrect. The correct pinouts are shown above.


Schneider Electric Nigeria