Search FAQs
Supplemental Profibus Island Module Health Bit Information for ACS Online Help
Goals and Symptoms
Information in this resolution applies to Structure of the STB NDP 2212 Diagnostic Message, Bytes 16 - 31 located in the Advantys Configuration Software Online Help > Hardware Help > Advantys STB Profibus DP NIM > Fieldbus Communication Support > Diagnostics Service. The purpose is to explain module conditions which are represented by the 0s and 1s in those bytes.
Causes and Fixes
This information may also be found on Pl@net in the Advantys STB Profibus DP Network Interface Applications Guide, p/n 890USE17300.
Legacy KB System (APS) Data: RESL179562 V1.0, Originally authored by WeDa on 09/01/2006, Last Edited by WeDa on 09/01/2006
Related ranges: Advantys STB
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: