Search FAQs
What is the cable part number to connect a Quantum with a 9 pin Sub-D serial port to a TSXCUSB232?
Issue:
Cable part number to connect a Quantum with a 9 pin Sub-D serial port to a TSXCUSB232
Product Line:
Quantum PLC
Resolution:
The Quantum DB9 RS-232 programming cable for that adapter is available in two lengths:
990NAA26320.....12 feet (3.66 meters)
990NAA26350.....50 feet (15.24 meters)
Cable part number to connect a Quantum with a 9 pin Sub-D serial port to a TSXCUSB232
Product Line:
Quantum PLC
Resolution:
The Quantum DB9 RS-232 programming cable for that adapter is available in two lengths:
990NAA26320.....12 feet (3.66 meters)
990NAA26350.....50 feet (15.24 meters)
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: