{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you disable a section in Unity Pro?

Right click on the section name and choose <properties>. Go to the <condition> tab. Enter a boolean reference or variable which can conditionally disable/enable the section. When this bit is ON, the section is enabled. When this bit is OFF, the section is disabled as indicated by a red mark on the dotted line leading to the section name.
When the bit is Forced ON or OFF, an 'F' is displayed over the red or green dot.


Schneider Electric Nigeria