Search FAQs
STBACO0220 Incorrect Wiring Diagram in the Advantys Hardware Components Reference Guide, 890USE17200
Issue
The purpose of this resolution is to inform users of the STBACO0220 analog output module that the wiring diagram is incorrect in the 'Advantys Hardware Components Reference Guide', part number 890USE17200.
The diagram in the Advantys Hardware Components Reference Guide dated 10-2006 and earlier, incorrectly shows the field device polarity for a current loop.
Product Line
Advantys STB
STBACO0220
Environment
Resolution
The following diagram correctly shows the field device polarity for a current loop.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: