{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
STBACO0120 Incorrect Wiring Diagram in the Advantys Hardware Components Reference Guide, 890USE17200

Issue
The purpose of this resolution is to inform users of the STBACO0120 analog output module that the wiring diagram is incorrect in the 'Advantys Hardware Components Reference Guide', part number 890USE17200.


Product Line
Advantys STB
STBACO0120


Environment


Resolution
The diagram in the Advantys Hardware Components Reference Guide dated 10-2006 and earlier, incorrectly shows the field device polarity for a current loop.


The following diagram correctly shows the field device polarity for a current loop.


Schneider Electric Nigeria