{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
STB Extended Temperature Range NIM Identification

Issue

The purpose of this resolution is to assist in identification of STB Extended Temperature Range Network Interface Modules.

Product Line
Advantys, STB

Resolution

Product Version numbers of the Extended Temperature Range Network Interface Modules (NIMs) are:
MODEL PV:

STBNCO2212 12
STBNDN2212 12
STBNDP2212 14
STBNFP2212 17
STBNIB2212 13
STBNIP2212 10
STBNMP2212 14

NIMs with the above minimum PV: values will be marked with the following Factory Mutual logo:



5VDC current ratings for NIMs with this marking and minimum PV: values are:

1.2A from -25° to +60°
575mA from +60°C to +70°C

Causes and Fixes

Reference Facts and Changes for information.


Legacy KB System (APS) Data: RESL190463 V1.0, Originally authored by WeDa on 12/27/2007, Last Edited by WeDa on 12/27/2007
Related ranges: Advantys STB

Schneider Electric Nigeria