{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Catalog 48332-EN_Ver5.0, 'Ethernet in Machines and Installations', Incorrect Switch Descriptions and Model Numbers Listed on Page 13

Issue
Page 13 of the catalog 48332-EN_Ver5.0 (filename: en5.0_48332.pdf) lists TCSESM163F23F0 as having 14 copper and 2 fiber ports and the TCSESM163F2CU0 as having 16 copper only for Connexium Managed switches. This is incorrect, the descriptions are reversed. TCSESM163F2CU0 should be 14 x 10/100BASE-TX ports and 2 x Fiber ports and TCSESM163F23F0 should be 16 copper only .
This page shows the incorrect switch Descriptions and Reference numbers (highlighted).


Product Line
Connexium
TCSESM163F23F0
TCSESM163F2CU

  • frgthy


Environment

Resolution
This page shows the correct Description and Reference numbers.

  • erft

Legacy KB System (APS) Data: RESL190814 V1.0, Originally authored by DaDz on 01/25/2008, Last Edited by DaDz on 01/25/2008
Related ranges: ConneXview, ConneXium - Ethernet

Schneider Electric Nigeria