{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
'140NOA6xxxx Interbus-S' modules are not recognized in the traffic cop.

Issue
'140NOA6xxxx Interbus-S' modules are not recognized in the traffic cop.

Product Line
Proworx32 V2.1

Environment
Windows 10

Resolution
The '140 NOA6xxxxx Interbus-S' modules are displayed in the traffic cop with a black question mark
inside a yellow circle when 'ProWORX 32' is connected to the PLC. (The module functions correctly).

The reason for this is because the status information is not provided by the executive firmware of the
'140 NOA6xxxxx Interbus-S' module. Since there is no status information for the 'ProWORX 32' traffic
cop to use, it doesn't know the module type and displays a question mark.


Legacy KB System (APS) Data: RESL191702 V1.0, Originally authored by AlCh on 05/12/2008, Last Edited by AlCh on 05/12/2008
Related ranges: ProWORX

Schneider Electric Nigeria