{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Maximum torque for the connections of the time relays RE11. Maximum length that you could peel the cable ?

Goals and Symptoms

Maximum torque for the connections of the time relays RE11.
Maximum length that you could peel the cable ?

Causes and Fixes

The maximum torque for the connections of the time relays RE11 is 1Nm, screew M3 / CEI 947-1
The maximum cable peeling length for connexion is 8mm.


Legacy KB System (APS) Data: RESL192132 V1.0, Originally authored by LaBe on 06/16/2008, Last Edited by LaBe on 06/16/2008
Related ranges: Zelio Time

Schneider Electric Nigeria