{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
STB Module Logic Bus Current Requirements

Goals and Symptoms

The purpose of this resolution is to provide information sources for STB module logic bus current consumption values used by Advantys Configuration Software v4.0.

Facts and Changes

This information can be found:
1. On line in v4.0 configuration software under Hardware Help in the Advantys STB Planning and Installation folder section highlighted below.



2. On line in v4.0 configuration software under Hardware Help. The four folders shown have logic bus current consumption values in individual modules Specification sections.



3. On Pl@net in the Advantys STB Technical publications listing.



The Advantys STB System Planning and Installation Guide, p/n 31002947 has information in the same location as the online version, ie: under STB Module Operating Temperature Ranges.

4. On Pl@net in the Advantys STB Technical publications listing. STB module manuals have logic bus current consumption values in the individual modules Specification sections.

Pl@net manuals are:

Analog I/O Modules Reference Guide 31007715
Digital I/O Modules 31007720
Special Modules Reference Guide 31007730
Counter Modules 31007725

There are errors in the System Planning and Installation Guides, Special Modules Reference Guides and Analog Module Reference Guides.

Online and Pl@net versions of the System Planning and Installation Guide incorrectly lists:
- STBXBE2100 current as 1mA (should be 100mA).

Online and Pl@net versions of the Special Modules Reference Guide:
- do not have bus current listed for the STBXBE1100 (25mA).

Online and Pl@net versions of the Analog Module Reference Guide incorrectly lists
- STBACO0120 current as 210mA (should be 155mA)

Attached is a quick reference listing of STB module logic bus current requirements.

reso_current.zip

Causes and Fixes

See Facts and Changes


Legacy KB System (APS) Data: RESL192962 V3.0, Originally authored by WeDa on 10/11/2008, Last Edited by WeDa on 11/25/2008
Related ranges: Advantys STB

Schneider Electric Nigeria