{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Modbus Error 161 gets returned when trying to connect with 'ProWORX 32'

Issue
Modbus error 161 gets returned when trying to connect to a Modicon PLC with 'ProWORX 32'

Product Line
'ProWORX 32', 'ProWORX NxT', 'Modsoft' and 'Concept'.

Environment
Windows 7

Resolution
'Modbus error 161' is defined as an invalid address or address range.

To resolve the problem:
1.) Check the address and communications parameter setup to ensure that they are correct.
2.) Check the Modbus cable to see if the DSR connection is asserted high.
3.) Try placing the PLC into Dim Awareness and use the 'PLC & I/IO Status' function in Modsoft to
view the status. (If this is successful, download to the PLC using the default parameters of
(Modbus address, RTU, 8, Even, 1, 9600).

Schneider Electric Nigeria