Search FAQs
RS485 pinout for the ATS48 to the TCESQM113M13M
Issue
RS485 pinout for the ATS48 to the TCESQM113M13M
Product Line
TCESQM113M13M
Environment
Windows 7
Resolution
The following RS-485 pinout can be used to connect the ATS48 to the TCESQM113M13M
ATS48 TCESQM113M13M
Pin 4 --------------------------- Pin 4
Pin 5 --------------------------- Pin 5
Pin 8 -------------------------- Pin 8
|---- Pin 6
jumper
|----- Pin 8
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: