{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

NIM Replacement Precaution When CANbus Baud Rate is Configured for 500k

Issue

The purpose of this resolution is to alert STB users to a precaution that should be observed when replacing a Network Interface Module (NIM).The error will occur when the original NIM and replacement NIM baud rate settings are different, ie: 500kbps and 800kbps respectively, or vice-versa. A power cycle of the entire island will clear the error if it occurs.

Product Line
Advantys,STB

Resolution

When replacing NIM's in islands that contain STBCPS2111 power supplies, or EOS-BOS combinations, it is recommended to remove power from all of these devices, rather than only the NIM. This is to prevent a possible NIM fatal error from occurring when power is restored. In the event this happens, it will not be possible to communicate with the island or perform an Autoconfigure with the RST button.

Causes and Fixes


Legacy KB System (APS) Data: RESL197949 V1.0, Originally authored by WeDa on 03/04/2009, Last Edited by WeDa on 03/04/2009
Related ranges: Advantys STB

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: