Search FAQs
What is the type of CF card used by the Magelis XBTGT7340 ?
Issue
What type of CF card can be used by the Magelis XBTGT or XBTGK Series of HMI?
Product Line
Magelis XBTGT, XBTGK
Environment
Physical HMI
Resolution
For Data Storage of Logging, Alarm Logs, Recipes, etc, the XBTGT and XBTGK series of HMI uses TYPE-II CF cards with a maximum capacity of 16GB formatted as Fat 32.
What type of CF card can be used by the Magelis XBTGT or XBTGK Series of HMI?
Product Line
Magelis XBTGT, XBTGK
Environment
Physical HMI
Resolution
For Data Storage of Logging, Alarm Logs, Recipes, etc, the XBTGT and XBTGK series of HMI uses TYPE-II CF cards with a maximum capacity of 16GB formatted as Fat 32.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: