{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to configure the STBEHC3020 for modulo mode

Issue
How to configure the STBEHC3020 for modulo mode.

Product Line
All versions of the Advantys Configuration Software.

Environment
Windows 7

Resolution
Connect the 'STBEHC3020' to the incremental encoder and configure the parameters in the Advantys Configuration software using the following instructions:.




  • Double click on the 'STBEHC3020' module to open the properties window for the module.


· Configure the parameters as shown.
· Download the application to the island.


· Start the PLC.
· Place the PLC into test mode.


Set the Input Validation bits to Off.


Set the Counter Enable to On.


Set the Counter Sync bit to On.


To reset the counter, toggle the counter sync bit from 0 to 1.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: