{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the meaning of the error 0X4BE in the error log of the 174CEV20040?

Issue

What is the meaning of the error 0X4BE in the error log?

Product Line

ConneXium - Ethernet

Environment

174CEV20040

Resolution

Error 0x4BE (1214 in decimal, or ERROR_INVALID_NETNAME), when returned from the MB+ driver, it indicates that you are trying to talk to a
nonexistent MB+ node. The Ethernet driver and the bridge software do not generate this error code. Check the routing to see if there is a node called out that is not actually on the network.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: