{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
140NOE77111 Firmware History for firmware versions 6.0, 5.6, 5.5, 5.1, 5.0, 4.8, and 4.7

Release Notice

This Resolution contains the Firmware History for the 140NOE77111 Exec firmware version 6.0 and earlier.

Goals and Symptoms

The attached document describes the Issues, Results, and Customer Actions of the changes to Exec versions 6.0, 5.6, 5.5, 5.1, 5.0, 4.8, and 4.7.

Facts and Changes

PRODUCTS Affected:

  • 140NOE77111

Causes and Fixes

Refer to the attached document for the complete details.

Attachments

NOE77111 Exec v6.0 Release Notes.zip

(Removed File URL: 202381_ED12/NOE77111_v6.0_Release_Notes_20130329.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/fad4e175266ecd60c1257b3e00160d68/fl_block_5/0.29E?OpenElement&FieldElemFormat=gif)

  • UPDATE 3/29/13 (doc revision 20130329)
    Firmware History for version 6.0 - excel format
  • UPDATE 12/21/2012
    zip file contains pdf's:
    1. Firmware History for version 5.6.
    2. Command 15 behavior
    3. Sub-Function 16 behavior
  • UPDATE 9/10/2012
    zip file contains pdf's:
    1. Firmware History for version 5.5.
    2. Command 15 behavior
    3. Sub-Function 16 behavior
  • UPDATE 12/15/2011
    zip file contains pdf's:
    1. Firmware History for version 5.1.
    2. Command 15 behavior
    3. Sub-Function 16 behavior
  • UPDATE 7/7/2011
    zip file contains pdf's:
    1. Firmware History for version 5.0.
    2. Command 15 behavior
    3. Sub-Function 16 behavior
  • UPDATE 12/22/10:
    1. Release of version 4.8.
    2. Added new title to section of Release Notes version 4.7; The NOE is incorrectly assigned an address of 'configured IP+1' instead of the 'configured IP' in a standalone 140CPU6716x.

Legacy KB System (APS) Data: RESL202381 V8.0, Originally authored by DaDz on 05/29/2010, Last Edited by DaDz on 03/30/2013
Related ranges: Modicon Quantum

Schneider Electric Nigeria

Attachment(s)
NOE77111_v6.0_Release_Notes_20130329.pdf [47.58 KB]